METHOD CheckCurrentSupportedCommunicationState : BOOL
This method checks if a specific DEVICE_TRANSITION_STATE can be processed in the current state.
Use IDevice2.CheckSupportedCommunicationState to check which DEVICE_TRANSITION_STATE is supported in general.
| InOut: |
|