IoDrvEtherNetIP.IOCycle (METH)

METHOD PUBLIC IOCycle

This method is called, when an EtherNet/IP Adapter is added to the project over an own IEC-Task. This method isn´t designed to get called from anywhere else.