TYPE IOL_Error : STRUCT
This datastructure contains the decoded error information of a failed IOL_CALL-FB execution
For details see:
[1] PI Specification, IO-Link Integration, Part 1, Version 1.0, December 2007, Order No. 2.812
[2] IO-Link Community, IO-Link Interface and System, V1.1.2, July 2013
| InOut: |
|