SubmoduleStatus (STRUCT)

TYPE SubmoduleStatus : STRUCT

Detailed information on the status of a single submodule.

Contains information wheather the module is available (exists ? is locked ?), the correct device type is configured, or if there is diagnostic information available.

InOut:

Name

Type

Comment

xDiagnosis

BOOL

A diagnostic entry is available/stored for this submodule (summary of xAdvice, xMaintenanceRequired/-Demanded, xFault).

xAdvice

BOOL

At least one Advice is available/stored for this submodule.

xMaintenanceRequired

BOOL

At least one requirement for maintenance is available/stored for this submodule.

xMaintenanceDemanded

BOOL

At least one demand for maintenance is available/stored for this submodule.

xFault

BOOL

At least one Fault is available/stored for this submodule.

ARInfo

SubmoduleState_ARInfo

IdentInfo

SubmoduleState_IdentInfo