class
IScriptProjectExtension.
IScriptProjectExtension
Bases: object
Provides extensions for IScriptProject
code_analysis
Access to code_analysis scripting API.
reset_memory_reserve_for_online_change
Resets the memory reserve for online change of all function blocks in the pool.
finish_load_project
Directs that a project is loaded completely.
is_project_load_finished
Returns whether the project has been loaded completely.
bool