The hexadecimal diagnostic codes listed here are output as WORD data type at the DiagCode output of the function block.
|
Code (hex) |
Description |
Options for remedy |
|---|---|---|
|
0000 |
The function block is not active. The Activate input is FALSE. |
Activate the function block by setting Activate to TRUE. |
|
8000 |
The function block is in a normal operating state. The muting process is not active (S_MutingActive = SAFEFALSE). The safety-related equipment of the zone of operation signals the defined safe state (S_AOPD_In = SAFETRUE). The enable signal is active (S_AOPD_Out = SAFETRUE). |
In case of an unexpected combination at the function block inputs relative to the physical input of the sensors, verify the connected hardware if required and correct the error. |
|
8001 |
The function block was activated. The start-up inhibit of the function block is active. |
Perform a reset on the function block to exit the active start-up inhibit for the function block. |
|
8002 |
The muting process was not active but the safety-related equipment of the zone of operation signals the non-safe state (S_AOPD_In = SAFEFALSE). |
To exit the active start-up inhibit for the function block, perform a reset on the function block once you have removed the request for the safety-related function at S_AOPD_In. |
|
8005 |
The muting process is not active (S_MutingActive = SAFEFALSE). The safety-related equipment of the zone of operation signals the defined safe state (S_AOPD_In = SAFETRUE). The enable signal is not active (S_AOPD_Out = SAFEFALSE). This state is completed after one cycle of the Safety Logic Controller. |
In case of an unexpected combination at the function block inputs relative to the physical input of the sensors, verify the connected hardware if required and correct the error. |
|
8011 |
The muting process in conveying direction 1 was requested at MutingSwitch11 (MutingSwitch11 = TRUE, MutingSwitch12 = FALSE, MutingSwitch21 = FALSE and MutingSwitch22 = FALSE). MaxMutingTime monitoring has started. |
In case of an unexpected combination at the function block inputs relative to the physical input of the sensors, verify the connected hardware if required and correct the error. |
|
8012 |
The muting process in conveying direction 1 is active (MutingSwitch11 = TRUE and MutingSwitch12 = TRUE). MaxMutingTime monitoring is running. The safety-related equipment of the zone of operation is not evaluated. |
In case of an unexpected combination at the function block inputs relative to the physical input of the sensors, verify the connected hardware if required and correct the error. |
|
8112 |
The muting process in conveying direction 2 is active (MutingSwitch21 = TRUE and MutingSwitch22 = TRUE). MaxMutingTime monitoring is running. The safety-related equipment of the zone of operation is not evaluated. |
In case of an unexpected combination at the function block inputs relative to the physical input of the sensors, verify the connected hardware if required and correct the error. |
|
8122 |
The muting process in conveying direction 2 was requested at MutingSwitch22 (MutingSwitch11 = FALSE, MutingSwitch12 = FALSE, MutingSwitch21 = FALSE and MutingSwitch22 = TRUE). MaxMutingTime monitoring has started. |
In case of an unexpected combination at the function block inputs relative to the physical input of the sensors, verify the connected hardware if required and correct the error. |
|
C001 |
The function block has detected a static TRUE signal at Reset. |
Verify the reset control device and the associated wiring. The Reset signal must be set to FALSE. |
|
C003 |
The function block has detected an invalid SAFEFALSE signal at S_MutingLamp. |
- Verify the hardware (muting lamp). - The signal connected to S_MutingLamp must be SAFETRUE. - Perform a reset on the function block. |
|
C004 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C005 |
The function block detected an invalid value at MaxMutingTime. MaxMutingTime= 0-600s |
- Verify the value configured at MaxMutingTime. - Correct the incorrect value. The value should correspond to the results of your risk analysis. The limit values for parameters should be taken into account when performing your risk analysis. |
|
C006 |
The muting process was not completed before time monitoring for the maximum muting time set at MaxMutingTime elapsed. |
- Verify the muting process. - Verify the time value specified at MaxMutingTime. This value should correspond to the results of your risk analysis. - Verify the hardware. - Perform a reset on the function block when MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 are set to FALSE. |
|
C010 |
The function block has detected a static TRUE signal at Reset. |
Verify the reset control device and the associated wiring. The Reset signal must be set to FALSE. |
|
C014 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C020 |
The function block has detected a static TRUE signal at Reset. |
Verify the reset control device and the associated wiring. The Reset signal must be set to FALSE. |
|
C024 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C030 |
The function block has detected a static TRUE signal at Reset. |
Verify the reset control device and the associated wiring. The Reset signal must be set to FALSE. |
|
C034 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C040 |
The function block has detected a static TRUE signal at Reset. |
Verify the reset control device and the associated wiring. The Reset signal must be set to FALSE. |
|
C044 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C054 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C064 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C074 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C084 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C094 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C0A4 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C0B4 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C0C4 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C0D4 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C0E4 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C0F4 |
Invalid muting sequence detected. Muting was not requested or the muting process has just been completed. The muting sensors then change to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C104 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C114 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C124 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C134 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C144 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C154 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C164 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C174 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C184 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C194 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C1A4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C1B4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C1C4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C1D4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C1E4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C1F4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C204 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C214 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C224 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C234 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C244 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C254 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C264 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C274 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C284 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C294 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C2A4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C2B4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C2C4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C2D4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C2E4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C2F4 |
Invalid muting sequence in conveying direction 1. After requesting the muting process by MutingSwitch11 and MutingSwitch12, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C304 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C314 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C324 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C334 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C344 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C354 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C364 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C374 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C384 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C394 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C3A4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C3B4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C3C4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C3D4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C3E4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C3F4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C404 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C414 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C424 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C434 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C444 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C454 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C464 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C474 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C484 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C494 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C4A4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C4B4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C4C4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C4D4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C4E4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
C4F4 |
Invalid muting sequence in conveying direction 2. After requesting the muting process by MutingSwitch22 and MutingSwitch21, the muting sensors changed to the following invalid state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF04 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF14 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF24 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF34 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF44 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF54 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF64 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF74 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = FALSE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF84 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CF94 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CFA4 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CFB4 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = FALSE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CFC4 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CFD4 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = FALSE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CFE4 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = FALSE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |
|
CFF4 |
Invalid muting sequence detected. During an active muting process MutingEnable became FALSE. In this situation the muting sensors had the following state: MutingSwitch11 = TRUE MutingSwitch12 = TRUE MutingSwitch21 = TRUE MutingSwitch22 = TRUE |
- Verify the muting process. - Set MutingSwitch11, MutingSwitch12, MutingSwitch21 and MutingSwitch22 to FALSE. - Then perform a reset on the function block. |