Function: This command opens the Scale program dialog box where the scaling of the CNC path is configured.
Call: Menu bar: CNC .
Requirement: A CNC path is open in the editor.
Restriction
Dialog box 'Scale program'
Scaling the CNC path is possible under the following conditions:
No usage
of axis A, B, or C
of variables
See also
Using Variables
Scaling factor
Preset: 0.001
0.001
Condition: Scaling factor >= 1e-3
For a scaling factor > 1, it is upscaled.
Axes
: The axis is scaled.
D (tool radius)
: The tool radius D is scaled.
OK
The scaling is performed. The block numbers are assigned automatically.