Function: This command provides information about the selected object in the SVN repository. The SVN Information dialog opens for this purpose.
Call: Context menu:
Requirement: A versioned object (with SVN link) is selected in the object tree.
Example
Name: Device_4\Plc Logic\Application\PLC_PRG
URL: file:///D:/SVN repository/trunk/ControlABC.project/Device/Plc Logic/Application/PLC_PRG/svnobj
Repository Root: file:///D:/SVN repository/
Repository UUID: 185325d7-73eb-e54b-ab50-206aa23c8b42
Revision: 29
Node Kind: File
Schedule: Normal
Last Changed Author: a.mayer
Last Changed Rev: 8
Last Changed Date: 17.01.2017 12:33:51
Text Last Updated: 17.01.2017 12:33:51
Checksum: d5fb4d91ebaea06f26bcdb15942724d57932b6a3