Object: EtherCAT Master
This tab contains the master parameters that are defined in the device description file.
If the auto-configuration mode is activated in the Master dialog, then the parameters are set automatically here in accordance with the specifications from the device description file and the network topology. Nothing should be changed in the generic editor, since an invalid configuration can be set here.
Value |
Editable, change is only effective if auto-configuration mode is deactivated. Whether or not the change becomes effective depends on the respective parameter. |
See also