Tab 'EtherCAT Slave - CoE Online'

Object: EtherCAT Slave

This tab shows the object index of the ESI file or the slave.

Requirement: The application is in online mode. The expert settings in the dialog box Slave must be enabled and the slave must support CoE.

Read objects

The object index is read one time.

Auto update

The objects are read in cycles.

Offline from ESI file

The dialog shows the contents of the object index from the device description.

Online from device

The dialog shows the contents of the object index from the device. SDOInfo must be enabled in the ESI file.

Flags

  • RO: Value is write-protected

  • RW: Value can be changed

Type

Data type of the parameter

Value

This value can be edited by double-clicking into the text field.