Object: EtherCAT Slave
This tab provides a different and more detailed view of the process data that is also displayed in the Process Data dialog box. Downloads are also selected here for PDO assignment and PDO configuration.
Requirement: The check box for the expert settings of the slave is selected.
See also:
List of PDOs that are assigned to the selected Sync Manager |
|
If a check box is selected, then the PDOs are activated and I/O channels are created. This is similar to the simple PDO configuration window. |
List of PDOs that are assigned to the selected Sync Manager |
|
You can add new PDOs or edit or delete existing PDOs by executing the respective commands (Add, Delete, Edit) in the command bar or shortcut menu. |
Name |
|
Index |
|
Direction |
|
Flags |
|
Exclude PDOs |
It is possible to define an exclusion list. When one PDO is active in the PDO Assignment, other PDOs are inactive and cannot be activated. |
Sync unit |
ID of the sync manager where the PDO should be assigned |
Displays the contents of the PDOs that are selected in the PDO List. You can add new entries or edit or delete existing entries by executing the respective commands (Add, Delete, Edit) in the command bar or shortcut menu. You can change the PDO order by clicking Move Up and Move Down. |
PDO assignment |
|
PDO configuration |
|
Load PDO info from the device |
The current PDO configuration is read from the slave and entered into the configuration. The lists in the upper and lower right are then deleted and filled with the read data. This is especially useful when the ESI file is incomplete and the configuration is available only on the slave. |
See also