Ethernet Adapter Configurator

Note

Refer to the general description for information about the following tabs of the device editor.

Only in the case of special features is there an additional help page for the specific device editor.

If the "<device name> Parameters" tab is not shown, then select the Show generic device configuration editors option in the CODESYS options (Device Editor category).

The CODESYS Ethernet adapter is used as a parent node for devices that use Ethernet-based protocols. CODESYS currently supports EtherNet/IP, Modbus, and PROFINET IO.

You insert the Ethernet adapter below the controller. Then you add the Ethernet-based fieldbus below the adapter.

See also