PROFIBUS DP Slave - 'Diagnosis'

The diagnosis data of the slave is displayed in this tabbed page. This information is useful for error checking.

Station status

DP_StationStatus 1-3 according to PROFIBUS DP specification

Master address

Address of the station address of the PROFIBUS DP master (if connected); otherwise 0xFF

IdentNr

ID number of the slave (as defined in associated GSD file)

Extended diagnosis

Extended diagnosis data according to PROFIBUS DP specification (IEC 61158-6). The channel-specific diagnosis is itemized using the GSD file and displayed as text.