PROFINET Module - Status

Object: PROFINET Module

This tab shows the diagnostics data and the alarms of the module.

Diagnostics Data

The diagnostics currently located in the device. The current diagnostics data is reloaded from the status display as long as a link can be established to the device.

Alarms

All alarms of this module that have been reported by this device since the start of the application. The alarms are stored in a ring buffer on the controller.

Acknowledge

Deletes the alarms from the ring buffer.

See also