Function: the command makes further commands available. It is used for the alignment of visualization elements in the window area of the visualization.
Call: Menu
, context menuSee also
Symbol:
Function: the command aligns the selected visualization elements along a line through the left-hand edge of the element that is positioned furthest left.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: the command aligns the selected visualization elements along a line through the upper edge of the element that is positioned highest.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: the command aligns the selected visualization elements along a line through the right-hand edge of the element that is positioned furthest right.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: the command aligns the selected visualization elements along a line through the lower edge of the element that is positioned lowest.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: the command aligns the selected visualization elements to their common vertical center.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command aligns the selected visualization elements to their common horizontal center.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command aligns the selected visualization elements so that the elements positioned furthest left and furthest right retain their position and the elements between them are positioned with the same horizontal spacing.
Call: Menu
, context menuRequirement: 3 or more elements are selected. The first element is blue, while the other elements are displayed in grey.
Symbol:
Function: The command aligns the selected visualization elements so that the blue element retains its position and the other elements are positioned with a larger horizontal spacing. The spacing increases by 1 pixel each time.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command aligns the selected visualization elements so that the blue element retains its position and the other elements are positioned with a smaller horizontal spacing. The spacing decreases by 1 pixel each time.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command aligns the selected visualization elements so that the blue element retains its position and the other elements are positioned with no horizontal spacing between them.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command aligns the selected visualization elements so that the uppermost and lowermost elements retain their position and the elements between them are positioned with the same vertical spacing.
Call: Menu
, context menuRequirement: 3 or more elements are selected. The first element is blue, while the other elements are displayed in grey.
Symbol:
Function: The command aligns the selected visualization elements so that the blue element retains its position and the other elements are positioned with a larger vertical spacing. The spacing increases by 1 pixel each time.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command aligns the selected visualization elements so that the blue element retains its position and the other elements are positioned with a smaller vertical spacing. The spacing decreases by 1 pixel each time.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command aligns the selected visualization elements so that the blue element retains its position and the other elements are positioned with no horizontal spacing between them.
Call: Menu
, context menuRequirement: Several elements are selected.
Symbol:
Function: The command makes the width of the selected visualization elements the same as the width of the blue selected element.
Call: Menu
, context menuRequirement: Several elements are selected. The first element is blue, while the other elements are displayed in grey.
The command does not work with lines or polygons.
Symbol:
Function: The command makes the height of the selected visualization elements the same as the height of the blue selected element.
Call: Menu
, context menuRequirement: Several elements are selected. The first element is blue, while the other elements are displayed in grey.
The command does not work with lines or polygons.
Symbol:
Function: The command makes the size of the selected visualization elements the same as the size of the blue selected element.
Call: Menu
, context menuRequirement: Several elements are selected. The first element is blue, while the other elements are displayed in grey.
The command does not work with lines or polygons.