Function: This dialog box is part of the wizard that opens when you create a new project with the HMI project template. It allows for the selection of the device type for the new project.
Call: Menu bar: HMI project)
(templateSee also
Window containing information about the selected device. |
|
|
List of installed HMI devices (with version) |
Show latest versions only |
|
Next > |
The selection is accepted and the Create HMI Project - Connect to HMI Panel dialog box opens. Requirement: The button is available only when you have selected an HMI device. |
Abort |
The configuration and settings of an HMI project are ended. |
See also