Symbol:
Tag: Special Controls
The element is used to link an existing ActiveX control in the visualization. You can configure the method calls and their parameters in the element properties of the ActiveX element.
In the CODESYS Store, you will find a sample project for using ActiveX components in visualizations.
See also
` CODESYS Store <http://store.codesys.com>`_
The position defines the location and size of the element in the visualization window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.
X |
X coordinate of the upper left corner of the element Specified in pixels.
Example: |
Y |
Y coordinate of the upper left corner of the element Specified in pixels.
Example: |
Width |
Specified in pixels.
Example: |
Height |
Specified in pixels.
Example: |
You can also change the values by dragging the box symbols () to other positions in the editor.
See also
The properties contain fixed values for the coordinates of the point of rotation. This point of rotation is shown as the symbol. The point is used as the center for rotating and scaling.
You can also change the values by dragging the symbols () to other positions in the editor.
The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.
Movement |
||
X |
Variable (numeric data type). Defines the X position (in pixels).
Example: Increasing this value in runtime mode moves the element to the right. |
|
Y |
Variable (numeric data type). Defines the Y position (in pixels).
Example: Increasing this value in runtime mode moves the element downwards. |
|
Rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees).
Example:
The midpoint of the element rotates at the Center point. This rotation point is shown as the In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right. |
|
Scaling |
Variable (integer data type). Causes centric stretching.
Example: The reference point is the Center property.
The value |
|
Interior rotation |
Variable (numeric data type). Defines the angle of rotation (in degrees).
Example: In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.
The rotation point is shown as the Note: If a static angle of rotation is specified in the property , then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed. |
|
You can link the variables to a unit conversion.
The properties X, Y, Rotation, and Interior rotation are supported by the "Client Animation" functionality.
See also
These method calls are executed during initialization. They are executed in the first cycle only.
These method calls are executed in every cycle. They are executed in the refresh rate of the visualization.
These method calls are executed in the refresh rate of the visualization. You define the call condition in the property
.
Method calls |
Button 'Create new' Creates a subnode below Methods with a call condition and parameters for the method call. |
Methods |
[<number>]
|
These properties are available only when you have selected the Preview: Support client animations and overlay of native elements option in the Visualization Manager.
Animation duration |
Defines the duration (in milliseconds) in which the element runs an animation
Animatable properties
The animated movement is executed when at least one value of an animatable property has changed. The movement then executed is not jerky, but is smooth within the specified animation duration. The visualization element travels to the specified position while rotating dynamically. The transitions are smooth. |
Move to foreground |
Moves the visualization element to the foreground
Variable (
Example:
|
See also
Requirement: User management is set up for the visualization.
Access rights |
Opens the Access rights dialog. There you can edit the access privileges for the element. Status messages:
|
See also