Visualization Element 'Rectangle', 'Rounded Rectangle', 'Ellipse'

Element properties

Element name

Optional

Example: Werkstueck_3

Hint: Assign individual names for elements so that they are found faster in the element list.

Type of element

Rectangle, Rounded Rectangle, Ellipse

Element property 'Position'

The position defines the location and size of the element in the visualization window. This is based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.

X

The x-coordinate of the upper left corner of the element

Specified in pixels

Example: 10

Y

The y-coordinate of the upper left corner of the element

Specified in pixels

Example: 10

Width

Specified in pixels

Example: 150

Height

Specified in pixels

Example: 30

Tip: You can change the values in X, Y, Width, and Height by dragging the corresponding symbols to another position in the editor.

Angle

Static angle of rotation (in degrees)

Example: 35

The element is displayed rotated in the editor. The point of rotation is the center of the element. A positive value rotates clockwise.

Tip: You can change the value in the editor by focusing the element to the handle. When the cursor is displayed as a rotating arrow , you can rotate the element about its center as a handle.

(1): Handle

Note: If a dynamic angle of rotation is also configured in the property Absolute movement ‣ Internal rotation , then the static and dynamic angles of rotation are added in runtime mode. The static angle of rotation acts as an offset.

See also

Radius setting

Visible only when Rounded Rectangle is selected in the Type of element property.

Radius

Rounding of the corners.

From style

Relative to the element size

Explicit: Allows for specifying a custom value in the Value setting.

Value

Radius of the rounded corners (in pixels)

Example: 5

Requirement: Explicit is selected in the Radius setting.

Element property 'Center'

The properties contain fixed values for the coordinates of the point of rotation. This point of rotation is shown as the symbol. The point is used as the center for rotating and scaling.

X

X-coordinate of the point of rotation

Y

Y-coordinate of the point of rotation

Note

You can also change the values by dragging the symbols () to other positions in the editor.

Element property 'Colors'

Normal state

The normal state is in effect if the variable in Color variables ‣ Toggle color is not defined or it has the value FALSE.

Frame color

Frame and fill color for the corresponding state of the variable.

Fill color

Transparency

Transparency value (0 to 255) for defining the transparency of the selected color.

Example: 255: The color is opaque. 0: The color is completely transparent.

Alarm state

The alarm state is in effect if the variable in Color variables ‣ Toggle color has the value TRUE.

Use gradient color

: The element is displayed with a gradient of two colors.

Gradient setting

The Gradient editor dialog box opens.

See also

Element property 'Appearance'

The properties contain fixed values for setting the look of the element.

Line width

Value in pixels

Example: 2

Note: The values 0 and 1 both result in a line weight of 1 pixel. If no line should be displayed, then the Line style property must be set to the option Invisible.

Fill attributes

The way in which the element is filled.

  • Filled:The element is filled with the color from property Colors ‣ Fill color .

  • Invisible: The fill color is invisible.

Line style

Type of line representation

  • Solid

  • Dashes

  • Dots

  • Dash Dot

  • Dash Dot Dot

  • not visible

Note

You can assign variables in the Appearance variables property for controlling the appearance dynamically. The fixed values here are overwritten.

See also

Element property 'Texts'

The properties contains character strings for labeling the element. The character string can also contain a placeholder with a format definition. In runtime mode, the placeholder is replaced by the current value in the specified format.

CODESYS accepts the specified texts automatically into the GlobalTextList text list. Therefore, these texts can be localized.

Text

Character string (without single straight quotation marks) for the labeling the element. Add a line break by pressing the keyboard shortcut Ctrl + Enter.

Example: Accesses: %i

The variable that contains the current value for the placeholder is specified in the property Text variable ‣ Text .

Tooltip

Character string (without single straight quotation marks) that is displayed as the tooltip of an element.

Example: Number of valid accesses.

The variable that contains the current value for the placeholder is specified in the property Text variable ‣ Tooltip .

See also

Element property 'Text properties'

The properties contain fixed values for the text properties.

Horizontal alignment

Horizontal alignment of the text within the element.

Vertical alignment

Vertical alignment of the text within the element.

Text format

Definition for displaying texts that are too long

  • Default: The long text is truncated.

  • Line break: The text is split into parts.

  • Ellipsis: The visible text ends with "..." indicating that it is not complete.

Font

Example: Default

: The Font dialog box opens.

: Drop-down list with style fonts.

Font color

Example: Black

: The Color dialog box opens.

: Drop-down list with style colors.

Transparency

Whole number (value range from 0 to 255). This determines the transparency of the respective color.

Example: 255: The color is opaque.

0: The color is completely transparent.

Please note: If the color is a style color and already has a transparency value, then this property is write-protected.

Element property 'Absolute movement'

The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.

Movement

X

Variable (numeric data type). Defines the X position (in pixels).

Example: PLC_PRG.iPos_X.

Increasing this value in runtime mode moves the element to the right.

Y

Variable (numeric data type). Defines the Y position (in pixels).

Example: PLC_PRG.iPos_Y.

Increasing this value in runtime mode moves the element downwards.

Rotation

Variable (numeric data type). Defines the angle of rotation (in degrees).

Example: PLC_PRG.iAngle1.

The midpoint of the element rotates at the Center point. This rotation point is shown as the symbol.

In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right.

Scaling

Variable (integer data type). Causes centric stretching.

Example: PLC_PRG.iScaling.

The reference point is the Center property.

The value 1 shrinks the element by a factor of 0.001. The value 1000 returns the element to its original size.

Interior rotation

Variable (numeric data type). Defines the angle of rotation (in degrees).

Example: PLC_PRG.iAngle2.

In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.

The rotation point is shown as the symbol.

Note: If a static angle of rotation is specified in the property Position ‣ Angle , then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed.

Use REAL values

Note: Only available if the device supports the use of REAL coordinates.

: The properties of the absolute movement are interpreted as REAL values. The values are not rounded.

The option allows for the individual fine-tuning of drawing the element, for example for the visualization of a smoother rotation.

Hint: If a horizontal or vertical line is drawn blurry on a specific visualization platform, then this can be corrected by an offset of 0.5px in the direction of the line thickness.

Note

You can link the variables to a unit conversion.

Note

The properties X, Y, Rotation, and Interior rotation are supported by the "Client Animation" functionality.

See also

Element property 'Relative movement'

The properties contains variables for moving the element. The reference point is the position of the element (Position property). The shape of the element can change.

Movement top-left

X

Variable (integer data type). It contains the number (in pixels) that the left edge is moved horizontally. Incrementing the value moves the element to the right.

Example: PLC_PRG.iDeltaX

Y

Variable (integer data type). It contains the number (in pixels) that the top edge is moved vertically. Incrementing the value moves the element to the down.

Example: PLC_PRG.iDeltaY

Movement bottom-right

X

Variable (integer data type). It contains the number (in pixels) that the right edge is moved horizontally. Incrementing the value moves the element to the right.

Example: PLC_PRG.iDeltaWidth

Y

Variable (integer data type). It contains the number (in pixels) that the bottom edge is moved vertically. Incrementing the value moves the element to the down.

Example: PLC_PRG.iDeltaHeight

See also

Element property 'Text variables'

These properties are variables with contents that replace a format definition.

Text variable

Variable (data type compliant with the format definition). It contains what is printed instead of the format definition.

Example: PLC_PRG.iAccesses

Note: The format definition is part of the text in the property Texts ‣ Text .

Note: If you specify a variable of type enumeration with text list support, then the name of the enumeration data type is added automatically in angle brackets after the variable name. Example: PLC_PRG.enVar <enumeration name>. Then the symbolic value of the enumeration component is printed instead of the numeric value when text is printed. Refer to the help page for the enumerations.

Tooltip variable

Variable (data type compliant with the format definition). It contains what is printed instead of the format definition.

Example: PLC_PRG.iAccessesInTooltip

Note: The format definition is part of the text in the property Texts ‣ Tooltip .

See also

Element property 'Dynamic texts'

Dynamic texts are variably indexed texts of a text list. At runtime, the text is displayed that is currently indexed in the variable.

Text list

Variable (string) or name of the text list as a fixed string in single straight quotation marks.

Example: 'Errorlist'

: Drop-down list with the dialogs available in the text lists.

Text index

Text list ID. This refers to the desired output text.

  • As fixed string with the ID in single straight quotation marks.

    Example: '1'

  • As a variable (STRING) for dynamically controlling the text output.

    Example: strTextID

    Sample assignment: PLC_PRG.strTextID := '1';

Tooltip index

Text list ID. This refers to the desired output text.

  • As fixed string with the ID in single straight quotation marks.

    Example: '2'

  • As a variable (STRING) for dynamically controlling the text output.

    Example: strToolTipID

    Sample assignment: PLC_PRG.strToolTipID := '2';

See also

Element property 'Font variables'

The variables allow for dynamic control of the text display.

Font name

Variable (STRING). Includes the font of the text.

Example: PLC_PRG.stFontVar := 'Arial';

The selection of fonts corresponds to the default Font dialog.

Size

Variable (numeric data type). Contains the font size (in pixels or points). The applied unit is specified in brackets after the variable name.

  • <pt>: Points (default)

    Example: PLC_PRG.iFontHeight <pt>

    Code: iFontHeight : INT := 12;

  • <px> : Pixels

    Example: PLC_PRG.iFontHeight <px>

    Code: iFontHeight : INT := 19;

If you click in the value field, a drop-down list opens on the right for setting the unit.

Hint: The font size is specified in points (example: Arial 12). Use points when the variable font size should match a font, for example if a font is set in the property Text property ‣ Font .

Flags

Variable (DWORD). Contains the flags for displaying fonts.

Flags:

  • 1: Italics

  • 2: Bold

  • 4: Underline

  • 8: Strikethrough

Note: You can combine the font displays by adding the coding of the flags. For example, a bold and underlined text: PLC_PRG.dwFontType := 6;

Character set

Variable (DWORD). Contains a character set number for the font.

The selection of character set numbers corresponds to the Script setting of the standard Font dialog.

Color

Variable (DWORD). Includes the color of the text.

Example: PLC_PRG.dwColorFont:= 16#FF000000;

Flags for text alignment

Variable (integer data type). Contains the coding for text alignment.

Example: PLC_PRG.dwTextAlignment.

Coding:

  • 0: Top left

  • 1: Horizontal center

  • 2: Right

  • 4: Vertical center

  • 8: Bottom

Note: You can combine the text alignments by adding the coding of the flags. For example, a vertical and horizontal centered text: PLC_PRG.dwFontType := 5;

Note

Fixed values for displaying texts are set in Text properties.

See also

Element property 'Color variables'

The Element property is used as an interface for project variables to dynamically control colors at runtime.

Toggle color

The property controls the toggled color at runtime.

Value assignment:

  • FALSE: The element is displayed with the color specified in the Color property.

  • TRUE: The element is displayed with the color specified in the Alarm color property.

Assignment options:

  • Placeholder for the user input variable

    • <toggle/tap variable>

    • <NOT toggle/tap variable>

    The color change is not controlled by its own variable, but by a user input variable.

    Note: Specify a variable for the mouse events Tap or Toggle in the input configuration of the element. Only then is the placeholder set. If you configure a variable in both Toggle and Tap, then the variable specified in Tap is used.

    Hint: Click the symbol to insert the placeholder <toggle/tap variable>. When you activate the Inputconfiguration, Tap FALSE property, then the <NOT toggle/tap variable> placeholder is displayed.

  • Instance path of a project variable (BOOL)

    Example: PLC_PRG.xColorIsToggeled

    Note: In the code, declare and implement the variable specified here. Its value assignment determines when the color changes.

Normal state

Alarm state

The properties listed below control the color depending on the state. The normal state is in effect if the variable in Color variables, Toggle color is not defined or it has the value FALSE. The alarm state is in effect if the variable in Colorvariables, Toggle color has the value TRUE.

Frame color

Assignment options:

  • Variable (DWORD) for the frame color

    Example: PLC_PRG.dwBorderColor

  • Color literal

    Example of green and opaque: 16#FF00FF00

Filling color

Assignment options:

  • Variable (DWORD) for the fill color

    Example: PLC_PRG.dwFillColor

  • Color literal

    Example of gray and opaque: 16#FF888888

Note

The transparency part of the color value is evaluated only if the Activate semi-transparent drawing option of the visualization manager is selected.

Note

Select the Advanced option in the toolbar of the properties view. Then all element properties are visible.

See also

Element property 'Appearance variables'

The properties contain IEC variables for controlling the appearance of the element dynamically.

Line width

Variable (integer data type). Contains the line weight (in pixels).

Fill attributes

Variable (DWORD). Controls whether the fill color of the element is visible.

  • Variable value = 0: Filled

  • Variable value > 0: Invisible; no fill color

Line style

Variable (DWORD). Controls the line style.

Coding:

  • 0: Solid line

  • 1: Dashed line

  • 2: Dotted line

  • 3: Line type "Dash Dot"

  • 3: Line type "Dash Dot Dot"

  • 8: Invisible; no line

Note

Fixed values can be set in the Appearance property. These values can be overwritten by dynamic variables at runtime.

See also

Element property 'State variables'

The variables control the element behavior dynamically.

Invisible

Variable (BOOL). Toggles the visibility of the element.

TRUE: The element is not visible at runtime.

Example: bIsVisible with VAR bIsVisible : BOOL := FALSE; END_VAR

Deactivate inputs

Variable (BOOL). Toggles the operability of the element.

TRUE: User inputs do not have any effect in runtime more. The element is shown as deactivated.

Note

The Invisible property is supported by the "Client Animation" functionality.

See also

These properties are available only when you have selected the Preview: Support client animations and overlay of native elements option in the Visualization Manager.

Animation duration

Defines the duration (in milliseconds) in which the element runs an animation

  • Variable (integer value)

    Example: Menu.tContent with VAR tContent : INT := 500; END_VAR

  • Integer literal

    Example: 500

Animatable properties

  • Absolute movement, Movement, X, Y

  • Absolute movement, Rotation

  • Absolute movement, Interior rotation

  • Absolute movement, Exterior rotation

The animated movement is executed when at least one value of an animatable property has changed. The movement then executed is not jerky, but is smooth within the specified animation duration. The visualization element travels to the specified position while rotating dynamically. The transitions are smooth.

Move to foreground

Moves the visualization element to the foreground

Variable (BOOL)

Example: bIsInForeground with VAR bIsInForeground : BOOL := FALSE; END_VAR

TRUE: At runtime, the visualization element is displayed in the foreground.

FALSE: At runtime, the visualization element is displayed in the layer where it was inserted in the visualization editor.

See also

Element property 'Input configuration'

The properties contain the configurations for the user input when using the mouse or keyboard. A user input defines an event and one or more actions that are executed when an event occurs.

The Configure button opens the Input Configuration dialog. There you can create or edit user inputs.

Configured user inputs are listed below the events. They each include the action that is triggered and the setting in short form.

Example: Execute ST Code: PLC_PRG.i_x := 0;

OnDialogClosed

Input event: The user closes the dialog.

OnMouseClick

Input event: The user clicks the mouse button completely in the element area. The mouse button is clicked and released.

OnMouseDown

Input event: The user clicks down on the mouse button.

OnMouseEnter

Input event: The user drags the mouse pointer to the element.

OnMouseLeave

Input event: The user drags the mouse pointer away from the element.

OnMouseMove

Input event: The user moves the mouse pointer over the element area.

OnMouseUp

Input events:

  • The user releases the mouse button within the element area. It is irrelevant whether the user has previously pressed the mouse button inside or outside the element area.

  • The user presses the mouse button within the element area, leaves the element area, and then releases the mouse button.

Note: This CODESYS-specific triggering behavior guarantees that actions for key elements are completed. A key element starts an action for OnMouseDown and ends the action for OnMouseUp.

Example: A visualization user presses the mouse button within the element area of the key element and then moves the cursor position so that it lies outside the element area. The action is ended anyway because OnMouseUp is triggered.

Tap

When a mouse click event occurs, the variable defined in Variable is described in the application. The coding depends on the Tap FALSE and Tap on enter if captured options.

Variable

Variable (BOOL) that is set on mouse click event.

Example: PLC_PRG.bIsTapped

TRUE: A mouse click event exists. It lasts as long as the user presses the mouse button over the element. It ends when the button is released.

FALSE: A mouse click event does not exist.

Requirement: The Tap FALSE option is not activated.

Tap FALSE

: The mouse click event leads to a complementary value in Variable.

TRUE: A mouse click event does not exist.

FALSE: While the mouse click event exists.

Tap on enter if captured

: During user input, it is also taken into consideration whether the mouse pointer is dragged within the element area or not while the mouse button is pressed.

TRUE: While the mouse click event exists and the mouse pointer is moved over the element area.

FALSE: A mouse click event does not exist. Or the user moves the mouse pointer outside of the element area while the mouse button is pressed.

The value is TRUE again as soon as the user moves the pointer back to the element area. The mouse is then captured.

Toggle

With the onset of a mouse click event, the variable is set; when the mouse click event is completed, the variable is reset.

Variable

Variable (BOOL). Its value toggled when the mouse click event is ended. This is when the user releases the mouse button while the mouse pointer is over the element area.

If the user releases the mouse button while the mouse pointer is outside of the element area, then the mouse click event is not ended and the value is not toggled.

Hint: The user can cancel a started toggle input by dragging the mouse pointer out of the element area.

Toggle on up if captured

: The value toggles regardless of where the mouse pointer is when the mouse button is released. The mouse is then captured.

Hotkey

Keyboard shortcut on the element for triggering specific input actions.

When the keyboard shortcut event occurs, the input actions in the Events property are triggered. In this way, it is not the input action itself that leads to this input action, but the mouse input action.

Key

Key pressed for input action.

Example: T

Note: The following properties appear when a key is selected.

Events

  • None

  • Mouse down: Pressing the key triggers the input actions that are configured in the OnMouseDown property.

  • Mouse up: Releasing the key triggers the input actions that are configured in the OnMouseUp property.

  • Mouse down/up: Pressing and releasing the key triggers the input actions that are configured in the OnMouseDown property and the OnMouseUp property.

Shift

: Combination with the Shift key

Example: Shift+T.

Control

: Combination with the Ctrl key

Example: Ctrl+T.

Alt

: Combination with the Alt key

Example: Alt+T.

Note

All keyboard shortcuts and their actions that are configured in the visualization are listed on the Keyboard Configuration tab.

See also

Element property 'Access rights'

Requirement: User management is set up for the visualization.

Access rights

Opens the Access rights dialog. There you can edit the access privileges for the element.

Status messages:

  • Not set. Full rights.: Access rights for all user groups : operable

  • Rights are set: Limited rights: Access is restricted for at least one group.

See also

See also