I_BIT_IN_*

This standard bit manipulation function contained in the <BIT_UTIL> library inverts a particular bit in the bit string applied at input IN.

NOTE:

Depending on the data type applied at input IN, the function I_BIT_IN_BYTE, I_BIT_IN_DWORD or I_BIT_IN_WORD has to be used.

Parameter

Data type

Description

IN

BYTE, WORD, DWORD (see note above)

Input bit string

BIT_NO

BYTE

Number (position) of the bit to be inverted

OUT

Same as data type at 'IN' (see note above)

Value with inverted bit BIT_NO