FUNCTION DeleteReceiver : ERROR
This function releases all ressources of a specific receiver.
When calling DriverClose all receivers connected to this driver are released automatically. Do not call DeleteReceiver afterwards!
Scope
Name
Type
Comment
Return
DeleteReceiver
ERROR
ERROR.NO_ERROR or appropriate error code
Input
hReceiverId
CAA.HANDLE
handle of receiver