GetReceiveCounter (FUN)

FUNCTION GetReceiveCounter : CAA.COUNT

Returns a counter which is incremented with each received message. Diagnostic Information can be also read by GetDiagnosis.

InOut:

Scope

Name

Type

Comment

Return

GetReceiveCounter

CAA.COUNT

number of received messages

Input

hDriver

CAA.HANDLE

handle of CAN interface

peError

POINTER TO ERROR

optional pointer to error enum