IsTransmitMessage (FUN)

FUNCTION IsTransmitMessage : BOOL

This function specifies whether a message was previously sent with Write.

InOut:

Scope

Name

Type

Comment

Return

IsTransmitMessage

BOOL

TRUE if messages is a Transmit CAN message.

Input

hMessage

CAA.HANDLE

handle of message

peError

POINTER TO ERROR

optional pointer to error enum