Machine Expert > V2.1 > Logiciel > Bibliothèques, Modèles et Exemples > Bibliothèques > CODESYS Libraries > CAA Can Low Level Extern Library Documentation > CAN Low Level > Functions > Internal > Basic Functions > _CreateIdAreaReceiver (FUN)

_CreateIdAreaReceiver (FUN)

FUNCTION _CreateIdAreaReceiver : CAA.HANDLE

Unmanaged implementation of CreateIdAreaReceiver

InOut:

Scope

Name

Type

Comment

Return

_CreateIdAreaReceiver

CAA.HANDLE

Input

hDriver

CAA.HANDLE

handle of CAN interface

xAlwaysNewest

BOOL

TRUE: returns only the newest message; FALSE: receiver with queue.

eEvent

CB.EVENT

trigger event when message received

xEnableSyncWindow

BOOL

use SYNC window: not implemented ==> do not care

peError

POINTER TO ERROR

optional pointer to error enum