FUNCTION _CreateSingleIdReceiver : CAA.HANDLE
Unmanaged implementation of CreateSingleIdReceiver
InOut:
|
Scope
|
Name
|
Type
|
Comment
|
Return
|
_CreateSingleIdReceiver
|
CAA.HANDLE
|
new receiver handle or CAA.gc_hINVALID in case of failure
|
Input
|
hDriver
|
CAA.HANDLE
|
handle of CAN interface
|
cobId
|
CL2I.COBID
|
id of message to be received
|
xRTR
|
BOOL
|
RTR bit
|
x29BitId
|
BOOL
|
29 Bit Id
|
xTransmit
|
BOOL
|
Transmit message
|
xAlwaysNewest
|
BOOL
|
TRUE: returns only the newest message; FALSE: receiver with queue.
|
eEvent
|
CB.EVENT
|
trigger event when message received
|
xEnableSyncWindow
|
BOOL
|
use SYNC window: not implemented ==> do not care
|
peError
|
POINTER TO ERROR
|
optional pointer to error enum
|
|