CanReconfigure (FUN)

FUNCTION CanReconfigure : BOOL

The function returns TRUE if itfNode can perform a Reconfigure-Action. Only nodes implementing IReconfigureProvider can be used as input of Reconfigure

InOut:

Scope

Name

Type

Return

CanReconfigure

BOOL

Input

itfNode

INode