FUNCTION_BLOCK Delete EXTENDS CBM.ETrig
This function block deletes a file.
Contrary to the original CAA specification the file may be deleted even if it is opened via ”FILE.Open”.
This behavior is dependent of the underlying operating system and file system.
InOut: |
|