FUNCTION GetProperty : DWORD
This function provides information on target-specific settings and functionalities, which concern the file or directory system or the implementation of optional function blocks.
|
Properties table |
|||
|
Nr. |
Constant name |
Meaning |
Return value |
|
function block – support |
|||
|
1 |
FILE_gc_PDIRRENAME |
Support of function block FILE_DirRename |
0: No 1: Yes |
|
2 |
FILE_gc_PRENAME |
Support of function block FILE_Rename |
0: No 1: Yes |
|
3 |
FILE_gc_PCOPY |
Support of function block FILE_Copy |
0: No 1: Yes |
|
4 |
FILE_gc_PSETATTRIBUTE |
Support of function block FILE_SetAttribute |
0: No 1: Yes |
|
Restrictions on directories and files |
|||
|
100 |
FILE_gc_PFILENAME83 |
Restriction of the directory and file names to 8.3 format |
0: No 1: Yes |
|
101 |
FILE_gc_PCAPITALLETTERS |
Restriction on capital letters for directory and file names |
0: No 1: Yes |
|
Path specification |
|||
|
200 |
FILE_gc_PABSOLUTEPATH |
Restriction on absolute path specification |
0: No 1: Yes |
|
201 |
FILE_gc_PDRIVELETTER |
Support of drive letters |
0: No 1: Yes |
|
210 |
FILE_gc_PRESOLVER |
Support of Resolver Syntax for file names |
0: No 1: Yes |
|
211 |
FILE_gc_PFTPRESOLVER |
Support of FTP-Client functions |
0: No 1: Yes |
|
212 |
FILE_gc_PHTTPRESOLVER |
Support of http-Client functions |
0: No 1: Yes |
|
Network |
|||
|
300 |
FILE_gc_PNETWORKDRIVES |
Support of network drives |
0: No 1: Yes |
| InOut: |
|