GetProperty (FUN)

FUNCTION GetProperty : DWORD

This function provides information on target-specific settings and functionalities, which concern the file or directory system or the implementation of optional function blocks.

Properties table

Nr.

Constant name

Meaning

Return value

function block – support

1

FILE_gc_PDIRRENAME

Support of function block FILE_DirRename

0: No

1: Yes

2

FILE_gc_PRENAME

Support of function block FILE_Rename

0: No

1: Yes

3

FILE_gc_PCOPY

Support of function block FILE_Copy

0: No

1: Yes

4

FILE_gc_PSETATTRIBUTE

Support of function block FILE_SetAttribute

0: No

1: Yes

Restrictions on directories and files

100

FILE_gc_PFILENAME83

Restriction of the directory and file names to 8.3 format

0: No

1: Yes

101

FILE_gc_PCAPITALLETTERS

Restriction on capital letters for directory and file names

0: No

1: Yes

Path specification

200

FILE_gc_PABSOLUTEPATH

Restriction on absolute path specification

0: No

1: Yes

201

FILE_gc_PDRIVELETTER

Support of drive letters

0: No

1: Yes

210

FILE_gc_PRESOLVER

Support of Resolver Syntax for file names

0: No

1: Yes

211

FILE_gc_PFTPRESOLVER

Support of FTP-Client functions

0: No

1: Yes

212

FILE_gc_PHTTPRESOLVER

Support of http-Client functions

0: No

1: Yes

Network

300

FILE_gc_PNETWORKDRIVES

Support of network drives

0: No

1: Yes

InOut:

Scope

Name

Type

Comment

Return

GetProperty

DWORD

Return value describes the property, see table.

Input

wProperty

WORD

Number of the property, see table.