PolarToCartesian (FB)

FUNCTION_BLOCK PolarToCartesian

This function block will change the polar coordinates of the two dimensional space to Cartesian coordinates , which are connected via:

InOut:

Scope

Name

Type

Comment

Input

lrAngle

LREAL

Angular coordinate (azimuth)

lrDistance

LREAL

Radius

Output

lrX

LREAL

X coordinate

lrY

LREAL

Y coordinate