UDP_Send (FB)

FUNCTION_BLOCK UDP_Send EXTENDS CBM.ETrigTo

This function block serves to sent data.

The content of the memory area indicated by pointer pData contains the data to be written. szSize defines the number of bytes to be written. When xDone is set to TRUE the data was written successfully.

The time out value has no effect at this function block.

InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts

Falling edge: Resets outputs

If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrigTo

udiTimeOut

UDINT

Defines the time (µs) after which an FB (e.g. requiring an external acknowledgement) aborts operation due to a timeout with error message.

ETrigTo

Output

xDone

BOOL

TRUE: Action successfully completed

ETrigTo

xBusy

BOOL

TRUE: Function block active

ETrigTo

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

ETrigTo

Input

hPeer

CAA.HANDLE

ipAddr

IP_ADDR

uiPort

UINT

szSize

CAA.SIZE

pData

CAA.PVOID

Output

eError

ERROR