IecTaskDisableScheduling (FUN)

FUNCTION IecTaskDisableScheduling : RTS_IEC_RESULT

Disable scheduling for the specified task

InOut:

Scope

Name

Type

Comment

Return

IecTaskDisableScheduling

RTS_IEC_RESULT

Returns the runtime system error code (see CmpErrors.library)

Input

hIecTask

RTS_IEC_HANDLE

Handle of the task