IecTaskEnableScheduling (FUN)

FUNCTION IecTaskEnableScheduling : RTS_IEC_RESULT

Enable scheduling for one specified task

InOut:

Scope

Name

Type

Comment

Return

IecTaskEnableScheduling

RTS_IEC_RESULT

Returns the runtime system error code (see CmpErrors.library)

Input

hIecTask

RTS_IEC_HANDLE

Handle of the task