FUNCTION UserMgrObjectAdd : RTS_IEC_HANDLE
Adds a new object to the user management, so the access rights can be configured on that object.
Note
The name of the object must include the full name-space with "Device" as the root node, e.g. "Device.MyObject" or if it's a file system object with "/" as the root node.
|
InOut:
|
|
Scope
|
Name
|
Type
|
Comment
|
|
Return
|
UserMgrObjectAdd
|
RTS_IEC_HANDLE
|
Handle to the object or RTS_INVALID_HANDLE if it could not be added
|
|
Input
|
pszObject
|
REFERENCE TO STRING
|
Full object name (see object tree)
|
|
pResult
|
POINTER TO RTS_IEC_RESULT
|
|
Pointer to error code
|
-
ERR_OK: Object could be added
-
ERR_PARAMETER: Object invalid = NULL or empty
-
ERR_NOTINITIALIZED: The user management is not initialized or it is not loaded yet
-
ERR_NOMEMORY: If memory could not be allocated to store this object
|
|
|