Machine Expert > V2.1 > Logiciel > Bibliothèques, Modèles et Exemples > Bibliothèques > CODESYS Libraries > CmpUserMgr Implementation Library Documentation > CmpUserMgr > Functions > Objecthandling > UserMgrObjectRemove (FUN)
FUNCTION UserMgrObjectRemove : RTS_IEC_RESULT
Removes an object from the user management and all its children
Scope
Name
Type
Comment
Return
UserMgrObjectRemove
RTS_IEC_RESULT
ERR_OK: Object could be removed
ERR_PARAMETER: Invalid object handle
Input
hObject
RTS_IEC_HANDLE
Handle to object