FUNCTION_BLOCK CREATE_ID
This function block creates a temporary ID from the physical identification of a slot of a PROFIBUS DP-slave or subslot of a PROFINET IO Device which can be used with the Communication Function Blocks.
In contrast to the other address conversion functions, it does not retrieve the ID from the projected devices of the application, but creates a temporary assignment of ID and the given address.
Use case is for example a Profinet implicit read-service. (RDREC without established connection CNCT)
Implementations may choose to only support a single or a limitted number of these temporary IDs and the underlying services.
Code-Example: Profinet implicit read
PROGRAM READ_Implicit
VAR
addr : CommFB.ADDR_TYPE;
createID : CommFB.CREATE_ID;
execRead : BOOL;
rdrec : CommFB.RDREC;
buffer : ARRAY[0..63] OF BYTE;
END_VAR
// init address:
// (this data might be retrieved by a bus-scan)
addr.SYSTEM := CommFB.IO_SYSTEM_TYPE.PROFINET_IO;
addr.PN.D.STATIONNAME := 'pnDevice'; // 'pnDevice' is some online device
addr.PN.D.INSTANCE := 1; // typically 0 or 1
createID(ADDR := addr);
IF(createID.ENO AND execRead) THEN
// Read data from profinet device
rdrec.ID := createID.ID; // ENO = TRUE, so the ID is valid and can be used for RDREC
rdrec.INDEX := TO_INT(16#AFF0); // I&M1-Data
rdrec.MLEN := TO_INT(SIZEOF(buffer));
rdrec.RECORD := ADR(buffer);
rdrec(REQ := execRead);
IF(rdrec.VALID OR rdrec.ERROR) THEN
//execution done
execRead := FALSE;
rdrec(REQ := execRead);
END_IF
END_IF
InOut: |