TYPE DP_AINFO : STRUCT
Alarm information of a profibus device (see: RALARM).
(see IEC 61158-6)
InOut:
|
Name
|
Type
|
Comment
|
D_LEN
|
BYTE
|
Length of the alarm information: 4 .. 63 bytes
|
ATYPE
|
BYTE
|
Alarm Type
|
SLOT
|
BYTE
|
Slot number
|
ASPEC
|
BYTE
|
Alarm Specifier
0: no further differentiation
1: Alarm appears and the related module is disturbed
2: Alarm disappears and the related module has no further errors
3: Alarm disappears and the related module is still disturbed
Bit 2: Additional acknowledge
Bit 3 to 7: Sequence number of alarm
|
ADD_INFO
|
ARRAY [0..58] OF BYTE
|
Additional alarm information
|
|