FUNCTION_BLOCK LConTlTo EXTENDS LConTl IMPLEMENTS ILConTlTo
Base implementation of a PLCopen Level Controlled Behavior Model (see: ILConTlTo) For use, this block should be extended and the specific inputs and outputs must be supplemented. The output eErrorID of the application-specific enum type ERROR must be added.
InOut:
|
Scope
|
Name
|
Type
|
Comment
|
Inherited from
|
Input
|
xEnable
|
BOOL
|
TRUE: Activates the defined operation FALSE: Aborts/resets the defined operation
|
LConTl
|
udiTimeLimit
|
UDINT
|
Max. operating time per invocation [µs], 0: No operating time limit
|
LConTl
|
Output
|
xDone
|
BOOL
|
TRUE: Ready condition reached
|
LConTl
|
xBusy
|
BOOL
|
TRUE: Operation is running
|
LConTl
|
xError
|
BOOL
|
TRUE: Error condition reached
|
LConTl
|
Input
|
udiTimeOut
|
UDINT
|
Max. operating time for executing [µs], 0: No operating time limit
|
|
|