FUNCTION GetID : DWORD
Get the ID of a Profinet Slave or Module from a DED.IDevice - object in the device tree.
This ID may be used for function blocks of the CommFB or ProfinetCommon libraries.
Scope
Name
Type
Comment
Return
GetID
DWORD
Input
pnDevice
DED.IDevice
A node in the device tree that is an instance of IDevice