FUNCTION_BLOCK PUBLIC FINAL TCP_Server EXTENDS LConC IMPLEMENTS IServer, IServer_Internal
Sets up a server over the ip and port specified in itfIPAddress and uiPort. A server can handle several connections. The output itfServer of these function block can be used to establish a connection via TCP_Connection.
|
InOut:
|
|
Scope
|
Name
|
Type
|
Initial
|
Comment
|
Inherited from
|
|
Input
|
xEnable
|
BOOL
|
|
TRUE: Activates the defined operation FALSE: Aborts/resets the defined operation
|
LConC
|
|
Output
|
xBusy
|
BOOL
|
|
TRUE: Operation is running
|
LConC
|
|
xError
|
BOOL
|
|
TRUE: Error condition reached
|
LConC
|
|
eErrorID
|
ERROR
|
|
|
LConC
|
|
Input
|
udiMaxConnections
|
UDINT
|
5
|
Maximum number of connections queued in TCP Stack
|
|
|
itfAsyncProperty
|
IAsyncProperty
|
|
|
|
|
itfTLSContext
|
ITLSContext
|
|
|
|
|
itfTSNContext
|
ITSNContext
|
|
|
|
|
itfIPAddress
|
IIPAddress
|
|
|
|
|
uiPort
|
UINT
|
|
|
|
|
Output
|
xActive
|
BOOL
|
|
|
|
|
itfServer
|
IServer
|
|
|
|
|