If not specified as a concrete formal parameter name, the term S_*_SafetyActive represents a common placeholder for the "safety-related function activated" outputs in this documentation. * stands as a placeholder for the actual safety-related function, e.g., STO or SOS. Accordingly, S_*_Request is used for the related function block request inputs.
The supported safety-related functions are described in detail in the topic "Safety Function (Basics)".
Output signals of the function block for signaling the currently activated safety-related function, i.e., the actual status of the safety-related drive module.
Data type: SAFEBOOL
Following activation, each S_*_SafetyActive output depends on the status of the applied safety-related function request signal and therefore on the status of the respective control device/sensor connected to the related S_*_Request input (activated/not activated, interrupted/not interrupted, open/close, depending on the used control device/sensor type) and also on whether or not the function block has detected an error or the start-up/restart inhibit is active.
Connection: Connect these outputs to other safety-related function/function blocks for further evaluation or to output terminals of your application.
Each S_*_SafetyActive output of this function block may only control the process directly if this does not adversely affect the safety-related function
WARNING | |
---|---|
Value |
Description |
---|---|
SAFETRUE |
The respective safety-related function is activated, i.e., the defined safe state has been achieved. The supported safety-related functions are described in detail in the topic "Safety Function (Basics)". The following conditions must be met:
Peculiarity for S_STO_SafetyActive: After indicating the active STO function, the axis coasts down. Therefore, S_STO_SafetyActive = SAFETRUE does not necessarily imply the standstill of the axis. The coast down time depends on physical properties of the used components, such as weight, torque, friction, etc. Refer to the hazard message below the table. |
SAFEFALSE |
The respective safety-related function is not activated ('normal operation'). This may be due to one of the following reasons:
|
WARNING | |
---|---|