Output for diagnostic message of the function block.
Data type: WORD
Connection: If required the signal can be connected to a standard variable of the WORD data type.
Function block-specific diagnostic and status messages are output via this output parameter and can be made available automatically to higher-level diagnostic tools.
The diagnostic code is specified as WORD data type. The respective hexadecimal value is specified in the "Diagnostic codes" help topic.