DCP_Error (ENUM)

TYPE DCP_Error :

Attributes:

qualified_only

InOut:

Name

Initial

Comment

NoError

16#0

requested data has been set

OptionNotSupported

16#1

requested optional Option is not supported

SuboptionNotSupported

16#2

requested optional suboption is not supported

SetNotPossible

16#3

set not possible for local reasons

ResourceError

16#4

temporary resource error within server

SetNotPossibleLocal

16#5

set not possible for local reasons

InOperation

16#6

set not possible because of operating application

Unknown

16#40000100

Unknown error

NotImplemented

16#40000101

Function not implemented (Client)

StackNotRunning

16#40000103

Stack not running.

NoResource

16#40000104

Out of ressources or ressource busy (Client)

InvalidInputs

16#40000105

Input-Parameter of DCP-Set/-Get Function Block is invalid

InvalidState

16#81814A00

Invalid State, Service not avaibale (e.g. already in progress, stack not running)

SendError

16#81814A01

Transmision not possible

Timeout

16#81814A02

Timeout, no response