IScriptBuildPropertiesExt

class

IScriptBuildPropertiesExt.

IScriptBuildPropertiesExt

Bases: object

Provides access to additional build properties (not part of the standard build_properties).

memory_reserve_for_online_change

Reserve additional space for function block instances to be used during online changes.

Type

int