State-controlled input for monitoring safety equipment.
Data type: SAFEBOOL
Initial value: SAFEFALSE
This input processes the status of the safety equipment (door open/closed). The signal present must be SAFETRUE so that the S_GuardLocked output can be switched to SAFETRUE (taking the other input signals into account).
Connection: Connect this input to a switch connected to the Safety Logic Controller (e.g., door or a separate, possibly positively-driven, single-channel or two-channel position switch), either directly or via other safety-related functions/function blocks.
If the function block is activated (input Activate = TRUE), the possible values at this input lead to the following function block behavior:
|
Value |
Description |
|---|---|
|
SAFETRUE |
The safety equipment is closed. The S_GuardLocked output can be switched to SAFETRUE, provided that the other input signals show the corresponding values (Activate = TRUE, S_GuardLock = SAFETRUE, no start-up/restart inhibit specified by means of S_AutoReset and S_StartReset) and the function block has not detected any errors. Refer to the hazard message below this table. |
|
SAFEFALSE |
The safety equipment is open. If SAFEFALSE is present at the S_GuardMonitoring input, the S_GuardLocked output is always SAFEFALSE, irrespective of all the other input signals. |
If no start-up/restart inhibit has been specified for the function block, the SAFETRUE status at the S_GuardMonitoring input can cause the S_GuardLocked output to immediately switch to SAFETRUE.
| WARNING | |
|---|---|
Irrespective of whether there is a single-channel or two-channel connection between the relevant position switch and the Safety Logic Controller, the S_GuardMonitoring input is only connected to one signal.
If a two-channel position switch is used, either the input channels of the safety-related input device must be parameterized accordingly or the safety-related SF_Equivalent or SF_Antivalent function block must be connected upstream for evaluating or monitoring the two-channel signal (e.g., SF_Equivalent function block, if the position switch features two N/C contacts).
Cross-circuit monitoring is not performed by the function block. It is your responsibility to perform this monitoring function outside of this function block in the safety-related control system.