|
Inout
|
ePos
|
SMC_BlockSearchPos
|
|
Position information. Requires connection to output ePos of SMC_BlockSearchSavePos
|
|
Input
|
bExecute
|
BOOL
|
FALSE
|
Risign edge: Enables the function block
|
|
bAbort
|
BOOL
|
FALSE
|
TRUE: Aborts the processing of the function block
|
|
bAppend
|
BOOL
|
FALSE
|
FALSE: Starts emptying poqDataOut on a rising edge at bExecute
|
|
poqDataIn
|
POINTER TO SMC_OUTQUEUE
|
NULL
|
Pointer to data of structure SMC_OUTQUEUE containing the path objects of typ SMC_GEOINFO, that are interpolated.
|
|
bStartFromSavedPos
|
BOOL
|
|
TRUE: Enables the function block to shorten the path from start up to the position, that is stored in SMC_BlockSearchPos .
FALSE: Disables the function block
|
|
nSizeOutQueue
|
UDINT
|
0
|
Size in bytes of the data buffer pbyBufferOutQueue, in which the path elements are copied. If the value is set, it may not be changed except after a reset.
|
|
pbyBufferOutQueue
|
POINTER TO ARRAY [0..0] OF SMC_GEOINFO
|
NULL
|
Pointer to the first byte of the storage area created for the path elements. If the value is set, it may not be changed except after a reset.
|
|
Output
|
bDone
|
BOOL
|
FALSE
|
TRUE: input date from poqDataIn have been precessed fully. After that, the function block performs no action until a reset is detected. When bExecute is set to FALSE, bDone is reset to FALSE.
|
|
bBusy
|
BOOL
|
FALSE
|
TRUE: Function block in execution
|
|
bError
|
BOOL
|
FALSE
|
TRUE: Error has occurred
|
|
wErrorID
|
SMC_ERROR
|
0
|
Error identification
Possible values
-
SMC_BS_SAVEDPOS_NOT_REACHED: Stored position has not been found. Probably wrong path.
-
SMC_BS_NO_POS_STORED: ePos contains no stored position. Possible cause is that SMC_BlockSearchSavePos was not executed or in a wrong way.
|
|
poqDataOut
|
POINTER TO SMC_OUTQUEUE
|
NULL
|
Pointer to data of structure SMC_OUTQUEUE containing the path elements of type SMC_GEOINFO that have been processed
|