FUNCTION SMC_GetLengthOfPrefix : LREAL
Calculates the length of the prefix of an object (from 0 to parameter value d). The object pg^ is not modified.
Scope
Name
Type
Return
SMC_GetLengthOfPrefix
LREAL
Input
pg
POINTER TO SMC_GEOINFO
d