SMC_SmoothBSpline (FB)

FUNCTION_BLOCK FINAL SMC_SmoothBSpline

Smoothes segments of consecutive G1 elements with a B-Spline of fifth degree. Each segment of at least 5 consecutive G1 elements of non-zero length is replaced by splines. The start and end positions of the G1 elements serve as control points of the B-spline that is created. Only the start position of the segment and the end position are interpolated exactly.

Each segment of n >= 5 G1 elements is replaced by n-5 polynomials.

Note
  • Does not support H-functions

  • Does not support changes of flags like G51, G52, G40 and so on, these changes are ignored

  • Requires 3D-Mode

  • Can be turned on and off from G-Code using G38/G39

  • A spline always contains the same tool correction information (i.e. lengths and diameter) as the first of the segments that it replaces.

Additional axis: First the values of the additional axis are also converted to a B-spline. For the linear axis (P,Q,U,V,W) only the positions at the end of each polynom are stored in SMC_GeoInfo. For the smoothed axis (A, B, C) the slope is also stored.

InOut:

Scope

Name

Type

Comment

Input

bExecute

BOOL

Execution starts on the rising edge.

poqDataIn

POINTER TO SMC_OUTQUEUE

Input path queue

nSizeOutQueue

UDINT

Size of the data buffer pbyBufferOutQueue in bytes.

pbyBufferOutQueue

POINTER TO ARRAY [0..0] OF SMC_GEOINFO

Points to the first byte of the memory area being allocated for the SMC_OUTQUEUE-structure. This area must be at least as big as defined in nSizeOutQueue. Typically the allocation of the memory buffer is done within the declaration part of the IEC-program by defining an array of SMC_GeoInfo (ExampleBuf: ARRAY[1..50] OF SMC_GEOINFO for a buffer which can hold 50 path` elements). After predefining the value it may be modified during a reset only.

eMode

SMC_SMOOTHBSPLINE_MODE

The element type applied for the smoothing of the axes.

wFeatureFlag

WORD

The feature bit (0..31) used for smoothing (controlled by G38/G39)

Output

bDone

BOOL

Will be set to TRUE as soon as the input data from poqDataIn has been ` processed completely. Thereafter, the module will not perform any further actions

bBusy

BOOL

TRUE, while execution of function block is not finished.

bError

BOOL

Signals, that an error has occurred within the function block.

wErrorID

SMC_ERROR

Error identification.

poqDataOut

POINTER TO SMC_OUTQUEUE

The queue for the output path