class
ScriptDeviceObject.
ScriptDeviceObjectMarker
class
ScriptDeviceObject.
ScriptDeviceObject
Bases: ScriptDeviceObject.ScriptDeviceObjectMarker
Functionality for manipulating device objects.
All device objects implementing DeviceObject will be extended with this methods.
get_device_identification
Gets the device identification.
enable
Marks this device as enabled during download.
disable
Marks this device as disabled during download.
is_enabled
Determines whether this instance is enabled during download.
bool
True if this instance is enabled during download; otherwise, False.
update
device=None
type=None
id=None
version=None
module=None
Updates the specified device.
WARNING | |
---|---|
device (DeviceId) -- The device Id.
type (int) -- The device type.
id (str) -- The device identification.
version (str) -- The device version.
module (str) -- The module ID.
plug
name
device=None
type=None
id=None
version=None
module=None
Plugs the specified device.
WARNING | |
---|---|
name (str) -- Name of the device.
device (DeviceId) -- The device Id.
type (int) -- The device type.
id (str) -- The device identification.
version (str) -- The device version.
module (str) -- The module ID.
add
name
device=None
type=None
id=None
version=None
module=None
Adds the specified device.
WARNING | |
---|---|
name (str) -- Name of the device.
device (DeviceId) -- The device Id.
type (int) -- The device type.
id (str) -- The device identification.
version (str) -- The device version.
module (str) -- The module ID.
insert
name
index
device=None
type=None
id=None
version=None
module=None
Inserts the specified device at the specified index.
WARNING | |
---|---|
name (str) -- Name of the device.
index (int) -- Index where to insert the device.
device (DeviceId) -- The device Id.
type (int) -- The device type.
id (str) -- The device identification.
version (str) -- The device version.
module (str) -- The module ID.
unplug
Unplugs the specified device.
get_simulation_mode
Gets the simulation mode.
True if simulation is enabled.
set_simulation_mode
simulation
Sets the simulation mode.
simulation (bool) -- if set to True, simulation is enabled.
get_gateway
Gets the gateway.
See also: ScriptDeviceObject.get_device_communication_settings
Guid
The guid of the gateway.
get_address
Gets the address of the device.
See also: ScriptDeviceObject.get_device_communication_settings
str
The device address in the bus independent CODESYS format.
set_gateway_and_address
gateway
address
Sets the gateway and address.
If you pass the empty guid and an empty address, the gateway address will be cleared. You can use ScriptGateway.find_address_by_ip() to search the CODESYS address when you know the ip address or hostname.
gateway (Guid, str or ScriptGateway) -- The gateway (Guid).
address (str) -- The address in the bus independent CODESYS format.
get_module_identification
Returns the unique identification of a module.
A module is a special type of device, that is only available within the context of a certain device. The module is identified by the same values as each owning device, with an additional module id, to distinguish it from other modules of the same device.
Examples for modules are device local io modules and similar nodes.
3.4.4.0
str
The module identification, or an empty string if this module has no module identification.
allow_interfaces_at
index
Get the name of the child interfaces that this device object can accept at the specified insert position.
3.5.4.0
index (int) -- The child index where a device should be inserted.
list
A list of possible interface names or None if no device can be inserted at that position.
device_parameters
Gets the set of device parameters.
Since V3.5.8.0, this actually is a ScriptMappableDeviceParameterSet.
3.5.4.0
connectors
Gets the connectors.
set_gateway_and_device_name
gateway
device_name
Sets the gateway and device name for communication.
If you pass the empty guid and an empty address, the gateway address will be cleared. The device will be tracked by its device name - when trying to go online, a quick online scan will be made and the first device with the given name will be selected.
3.5.8.0
gateway (Guid, str or ScriptGateway) -- The gateway, its Guid or its string representation.
device_name (str) -- The device name.
set_gateway_and_ip_address
gateway
ip_address
port=11740
Sets the gateway and IP address for communication.
3.5.8.0
gateway (Guid, str or ScriptGateway) -- The gateway, its Guid or its string representation.
ip_address (IPAdress or str) -- The IP Adress as a string. If port is omitted, the port can be passed here separated by a colon (e.G. "127.0.0.1:11739").
port (ushort) -- The port. Omit to use the default port 11740.
InvalidOperaionException -- If gateway is passed as a string and several gateways have the same name.
get_device_communication_settings
Gets the communication settings of the device.
export_io_mappings_as_csv
file_path
Export the io mappings as a CSV file to the specified absolute path.
3.5.8.0
file_path (str) -- The absolute path of the file to export.
import_io_mappings_from_csv
file_path
Imports the io mappings from a CSV file at the specified absolute path.
3.5.8.0
file_path (str) -- The absolute path of the file to import.
driver_info
Get the driver info of the device.
3.5.9.0
allow_symbolic_var_access_in_sync_with_iec_cycle
Property used by the symbol configuration to determine if symbolic variable access is allowed to be synchronized with the IEC cycle.
The default is False and should be kept for most use cases. Setting this to True may increase the jitter for all applications running on the device because the task accessing the variables may block other tasks. The device object has to support DeviceObject (3.5.10.0) to access the value.
3.5.10.0
bool
class
ScriptDeviceObject.
ScriptProjectDeviceExtension
Bases: object
Functionality to add top-level devices (e. G. SPS) to projects.
ScriptProject instances are amended with these objects.
3.4.3.0
add
name
device=None
type=None
id=None
version=None
module=None
Adds the specified device.
WARNING | |
---|---|
name (str) -- Name of the device.
device (DeviceId) -- The device Id.
type (int) -- The device type.
id (str) -- The device identification.
version (str) -- The device version.
module (str) -- The module ID.
class
ScriptDeviceObject.
DeviceId
Bases: object
Represents a Device ID.
An implementation class of this interface is injected under the name "DeviceID" into the python scope, so python code can create device IDs without the need to subclass that interface. The constructor signature is: DeviceID(int iType, string stId, string stVersion)
type
Type of the device.
int
id
Id of the device.
The format for this id is specified for each type. The id is unique within the class of devices of one type.
str
version
The version of the device.
The format for the version string is specified for each type.
str
class
ScriptDeviceObject.
ModuleId
Bases: ScriptDeviceObject.DeviceId
Unique identification for a module.
A module is a special type of device, that is only available within the context of a certain device. The module is identified by the same values as each owning device, with an additional module id, to distinguish it from other modules of the same device.
Examples for modules are device local io modules and similar nodes.
module_id
Id of the module.
The format for this id is specified for each type. The id is unique within the class of devices of one type.
str
class
ScriptDeviceObject.
ScriptCommunicationSettings
Bases: object
Provides access to the communication settings of the device.
gateway_guid
The guid of the gateway.
Guid
device_address
The address of the device.
str
prompt_at_login
Whether there's a prompt at login.
bool
secure_online_mode
Gets a boolean value indicating whether secure online mode is activated for the corresponding devices.
If set, user interfaces should prompt the user before an operation is executed which changes the state of the controller.
bool
device_name
Gets the name of the device as entered on the communication settings page.
str
monitoring_interval_msec
The interval for status and variable monitoring measured in milliseconds.
Default = 200ms, Minimum = 10ms, Maximum = 1000ms, Increment 10ms. Invalid values will be ignored
int
monitoring_interval
The interval for status and variable monitoring measured in milliseconds.
Default = 200ms, Minimum = 10ms, Maximum = 1000ms, Increment 10ms. Invalid values will be ignored
TimeSpan
TrackingMode
Property to get the mode used to track a device on the network - whether the device is tracked via CODESYS address, ip address or name.
DeviceTrackingMode
scanned_device_name
The name of the physical device (E.g. "MyPlc"), as seen in the network scan.
str
scanned_ip_address_and_port
Device IP Address and Port if block driver TCP is used for connection.
Format: "192.168.101.109:11740", as seen in the network scan.
This may return the emtpy string if it's not available. Even if some network scan members are set, this does not guarantee that all of them are set.
str
scanned_target_id
Target ID.
Format: "1234 ABCD" (=hexadecimal), same as in device description, as seen in the network scan.
This may return the emtpy string if it's not available. Even if some network scan members are set, this does not guarantee that all of them are set.
str
scanned_target_name
The name of the target (E.g. "CODESYS PLC Win NT"), as seen in the network scan.
This may return the emtpy string if it's not available. Even if some network scan members are set, this does not guarantee that all of them are set.
str
scanned_target_type
Target Type (Format: "4096" (=decimal), same as in device description), as seen in the network scan.
This may return the emtpy string if it's not available. Even if some network scan members are set, this does not guarantee that all of them are set.
str
scanned_target_vendor
The vendor of the target, as seen in the network scan.
This may return the emtpy string if it's not available. Even if some network scan members are set, this does not guarantee that all of them are set.
str
scanned_target_version
The version of the target, as seen in the network scan.
This may return the emtpy string if it's not available. Even if some network scan members are set, this does not guarantee that all of them are set.
str
is_communication_encrypted
Get or set if encrypted communication should be used with the device.
3.5.17.0
bool