ScriptDriverInfo

class

ScriptDriverInfo.

ScriptDriverInfo

Bases: object

Provides access to the driver info of the device.

Mostly the visible parts of the tab "PLC Settings" in the device editor.

can_set_io_application

Whether the IO application can be set.

Return type

bool

io_application

Get/set the object Guid of the application which does the IO handling.

Return type

Guid

set_io_application

application

Set the application which does the IO handling.

Parameters

application (ScriptApplication) -- Script object of the application.

update_ios_while_in_stop

Update IOs while in stop.

Return type

bool

behaviour_for_outputs_on_stop

Get/set the behaviour for outputs on stop.

Return type

StopResetBehaviour

user_program_for_stop_reset_behaviour

Get/set the behaviour program for stop/reset if behaviour_for_outputs_on_stop is set to ExecuteProgram.

See also: StopResetBehaviour.ExecuteProgram

Return type

str

always_update_variables

Set the mode for (always) updating variables.

bus_cycle_task_by_name

Get the name of the bus cycle task.

Return type

str

bus_cycle_task_by_guid

Get the object guid of the bus cycle task.

Return type

Guid

set_bus_cycle_task

name_guid_or_task

Set the bus cycle task by name or object guid or script object.

Parameters

name_guid_or_task (str or guid or ScriptObject) -- Name or Object Guid or Script Object of the task.

generate_force_variables

Generate force variables for IO mapping.

Return type

bool

enable_diagnosis

Enable diagnosis for devices.

Return type

bool

show_io_warnings_as_errors

Show IO warnings as errors.

Return type

bool

class

ScriptDriverInfo.

AlwaysUpdateVariablesMode

Bases: enum.Enum

Defines always mapping modes on a parameter or connectors.

Disabled

= 1

Disable the always update of the variables.

OnlyIfUnused

= 2

The io channel is mapped in the bus cycle task if no other task is using it. If it used in an task then alwaysmapping is ignored, because it is updated in the used task only.

AlwaysInBusCycle

= 3

The io channel is always updated in the bus cycle task independent of the real task usage. Therefore task consistency is not guaranteed.