ScriptSymbolConfigObject

class

ScriptSymbolConfigObject.

ScriptSymbolConfigObjectMarker

Bases: object

Every ScriptObject instance will be extended with this method.

Version added

3.5.10.0

is_symbol_config

Gets a value indicating whether this instance is a symbol config object.

Return type

bool

Returns

True if this instance is symbol config object, otherwise False.

class

ScriptSymbolConfigObject.

ScriptSymbolConfigObject

Bases: ScriptSymbolConfigObject.ScriptSymbolConfigObjectMarker

Functionality for manipulating symbol configuration objects.

Version added

3.5.10.0

client_side_layout_calculator_guid

Gets or sets the Guid denoting the currently configured client side layout calculator.

Currently, two different values are allowed: Guid.Empty to use the Compatibility Offset Calculator which is always available. And "{0141eb75-141b-4ea1-9a8c-75f952b22a6c}" to use the OptimizedOutputOffsetCalculator which is new with V3.5.7.0 and also requires the compiler version 3.5.7.0 (see http://jira.3s-software.com/browse/CDS-41816). This scheme may be extended to allow more or even arbitrary offset calculators in the future.

Return type

Guid

client_side_layout_calculator

Gets or sets the calculator object denoting the currently configured client side layout calculator.

Currently, two different values are allowed: Guid.Empty to use the Compatibility Offset Calculator which is always available. And "{0141eb75-141b-4ea1-9a8c-75f952b22a6c}" to use the OptimizedOutputOffsetCalculator which is new with V3.5.7.0 and also requires the compiler version 3.5.7.0 (see http://jira.3s-software.com/browse/CDS-41816). This scheme may be extended to allow more or even arbitrary offset calculators in the future.

available_client_side_layout_calculators

Gets all currently known layout calculators.

enable_direct_io_access

Gets or sets a boolean whether direct Access to the I/O Area is configured.

Enabling direct access to the I/O area is supported for debugging purposes, e. G. testing the cables and connections. It is not meant for productive operation. It is only available under certain conditions, e. G. the compiler version must be >= V3.5.8.0 and the symbol config must not be generated as a child application.

Return type

bool

check_effective_direct_io_access

Checks whether and why the direct Access to the I/O Area is effectively enabled / disabled.

Enabling direct access to the I/O area is supported for debugging purposes, e. G. testing the cables and connections. It is not meant for productive operation. It is only available under certain conditions, e. G. the compiler version must be >= V3.5.8.0 and the symbol config must not be generated as a child application.

Return type

DirectIoAccessObstacles

Returns

The DirectIoAccessObstacles flag describing which reasons prevent the Direct IO Access from being enabled.

get_direct_io_obstacle_explanations

obstacles

Gets user readable, localized messages / explanations of the obstacles.

Parameters

obstacles (DirectIoAccessObstacles) -- The obstacles.

Return type

list <str>

Returns

A list of strings with one entry for each obstacle, or an "is enabled" message when obstacles == DirectIoAccessObstacles.None.

content_feature_flags

The configured content feature flags. This is partially redundant with SymbolConfigObject.ExportCommentsInXML and SymbolConfigObject.SupportOPCUA.

Return type

SymbolConfigContentFeatureFlags

effective_content_feature_flags

The effective content feature flags, considering the content_feature_flags and the compiler version setting.

Return type

SymbolConfigContentFeatureFlags

get_symbol_configuration_xsd

Gets the current symbol configuration XML schema, as appropriate for the current symbol config object.

The schema is delivered as a byte array, containing the UTF-8 encoded XSD file as it is also published in the http://www.3s-software.com/schemas/Symbolconfiguration.xsd. The above URL aways points to the newest released version of the schema, while the get_symbol_configuration_xsd() property delivers the XSD file applicable to the current release of the SymbolConfig plugin.

Return type

list <byte>

Returns

The current symbol configuration XML schema as byte array.

symbol_attribute_filter_type

The configured filter type for the attributes.

Return type

SymbolAttributeFilterTypes

effective_symbol_attribute_filter_type

The effective filter type, considering compiler version and other side conditions.

Return type

SymbolAttributeFilterTypes

symbol_attribute_filter_data

Describes the filter data for SymbolAttributeFilterTypes.Prefix and SymbolAttributeFilterTypes.Regex.

Return type

str

symbol_comment_filter_type

The configured comment filter type.

Return type

SymbolCommentFilterType

effective_symbol_comment_filter_type

The effective comment filter type, considering compiler version and other side conditions.

Return type

SymbolCommentFilterType

get_all_signatures

compile=True

Get all signatures (compiler and configured).

Parameters

compile (bool) -- If True, build the application before generating the list. If the application was not built before, the returned list is empty.

Returns

Collection of signatures.

get_all_datatypes

compile=True

Get all data types (compiler and configured).

Parameters

compile (bool) -- If True, build the application before generating the list. If the application was not built before, the returned list is empty.

Returns

Collection of data types.

get_only_configured_signatures

Get only the configured signatures.

Returns

Collection of signatures.

get_only_configured_datatypes

Get only the configured data types.

Returns

Collection of data types.

class

ScriptSymbolConfigObject.

ScriptClientSideLayoutCalculatorDescriptionCollection

Bases: list

Descriptions of the client side layout calculators.

Version added

3.5.10.0

class

ScriptSymbolConfigObject.

ScriptClientSideLayoutCalculatorDescription

Bases: object

Description of an client side layout calculator.

Currently, two different values are allowed: Guid.Empty to use the Compatibility Offset Calculator which is always available. And "{0141eb75-141b-4ea1-9a8c-75f952b22a6c}" to use the OptimizedOutputOffsetCalculator which is new with V3.5.7.0 and also requires the compiler version 3.5.7.0 (see http://jira.3s-software.com/browse/CDS-41816). This scheme may be extended to allow more or even arbitrary offset calculators in the future.

Version added

3.5.10.0

type_guid

The unique ID of the output layout calculator.

Return type

Guid

name

The name of the output layout calculator - human readable and localized.

Return type

str

description

A longer description of the output layout calculator.

Return type

This may be shown in a tooltip, and should give some detailed explanation of the calculator, and e. G. the conditions under which the calculator is valid.

class

ScriptSymbolConfigObject.

ScriptSymbolConfigSignature

Bases: object

Signature element of the symbol configuration.

Version added

3.5.10.0

name

The name of this element.

Return type

str

full_qualified_name

The full qualified name of this element.

Return type

str

library_id

The identification of the library where this signature is declared.

Return type

str

namespace_path

Namespace path of the library where this signature is declared.

Return type

list <str>

variables

The variables of the signature.

Return type

ScriptSymbolConfigVariableCollection

class

ScriptSymbolConfigObject.

ScriptSymbolConfigSignatureCollection

Bases: list

Collection of symbol configuration signatures.

Version added

3.5.10.0

find

name

library_id=None

Get the first ScriptSymbolConfigSignature with the specified name and library ID which should be fully qualified.

Parameters
  • name (str) -- Name of a signature.

  • library_id (str) -- Library ID.

Returns

Signature of the symbol configuration. Otherwise None.

class

ScriptSymbolConfigObject.

ScriptSymbolConfigVariable

Bases: object

Variable element of the symbol configuration.

Version added

3.5.10.0

name

The name of this variable.

Return type

str

type

The type of this variable, as the user declared it.

Return type

str

comment

Gets the comment of the signature or variable, or an empty string if no comment is available.

This member is only valid for objects parsed from the compiler, not for configured symbol config instances.

Return type

str

configured_access

The allowed symbolic access to this variable.

Return type

SymbolAccess

maximal_access

The maximal access that is allowed for this variable, decided by the given attributes.

Return type

SymbolAccess

effective_access

The effective symbolic access to this variable.

Return type

SymbolAccess

exported_via_attribute

Gets a value indicating whether this variable is configured via compiler attribute.

Return type

bool

Returns

True if exported via attribute; otherwise False. If True, the Access attribute gives the effective access for this variable.

attribute_access

Gets the attribute access. When attribute_access is false, the result of this member is undefined.

Return type

SymbolAccess

type_library_id

Gets the library id, when the type of the member is from a library.

This is currently only set for supported data types (userdef and array).

Return type

str

full_qualified_base_type

Gets the full qualified base type of the member.

This is currently only set for supported data types (userdef and array).

Return type

str

alias_type

The name of the alias type.

For variables with aliased types, the Type, SymbolConfigVariable.VariableType and SymbolConfigVariable2.FullQualifiedBaseType properties point to the effective, resolved type. Use this member in the UI to display the alias type used in the source. This member is only valid for objects parsed from the compiler, not for configured symbol config instances.

Return type

str

class

ScriptSymbolConfigObject.

ScriptApplicationSymbolConfigExtension

Bases: object

Extension provider for ApplicationObject instances.

Version added

3.5.10.0

create_symbol_config

export_comments_to_xml

support_opc_ua

client_side_layout_calculator

Add the symbol configuration object to an application.

Return type
Returns

Script object of the symbol config object.

exception

ScriptSymbolConfigObject.

ScriptSymbolConfigInvalidObjectException

stMessage

Bases: Exception

Exception which is thrown when the symbol configuration object is modified externally and so the scripting objects are not valid anymore.

Version added

3.5.10.0